Hi for All,
I`m use MSCAN MC9S12XET256MAG.
Module MSCAN is interrupt driven with priority 3.
If I use additional timer interrupt with priority 5 than CAN messages is lost ( not passed ).
Why?
Best regards.
It can happen in case timer interrupt takes so long that all 5 receive buffers are filled with messages and you get overrun flag set. Is it the case? If so, then try triming your timer interrupt. If you can't ( though there are no reasons for that), then you can use interrupt nesting to fix the problem. To do so, reverse priorities. Long ISR's must have least interrupt priority. To make enormously long ISR's interrupted by higher priority interrupts, add asm("CLI") or enable_interrupts at top of long ISR's.
Hi, Kef.
TX CAN messages not transfered.
Timer interrupt is ECT and used FreeRTOS ( tick timer ) .
CAN TX interrupt don't disable global interrupt and so it is possible to switch context.
But this should not lead to loss TX messages, only additional delay?
And messages lost under heavy load CANbus ( with other node with a higher priority messages).
PS: It seems that the request for transfer of CAN messages
( in reg. CAN4TFLG ) is reset if the unit has lost arbitration on the bus.
No.
Show you code how do you send CAN messages.
Hello,
ISR is:
ISR(CANrez_InterruptTx){ byte buffer = (CAN4TFLG & CAN4TIER) & 7; /* Temporary variable */ CAN4TIER &= ~buffer; /* Clear appropriate transmit flags and release TX buffer */ if (CANrez_EnEvent) { /* Are events enabled? */ CANrez_OnFreeTxBuffer((word)buffer); /* If yes then invoke user event */ }}
Here is not disable global interrupt. And event handler:
void CANrez_OnFreeTxBuffer(word BufferMask){ /* Write your code here ... */ MsgCANbus msg_isr_tx_can; // сообщение CAN для передачи контроллеру portBASE_TYPE mng_woken = FALSE; // пробуждение менеджера unsigned char num_buf = 0; // номер используемого аппаратного буфера if ( uxQueueMessagesWaiting( q_isr_tx_can ) ) // CAN очередь не пустая { if ( 1 == ( CANrez_GetStateTX() & CAN4TFLG_TXE0_MASK ) ) // есть свободные { // Принимаем CAN сообщение от менеджера if ( pdPASS == xQueueReceiveFromISR( q_isr_tx_can, & msg_isr_tx_can, & mng_woken ) ) // прочитали сообщение { if ( MI_CANmng2isr == msg_isr_tx_can.id ) // сообщение от менеджера { CANrez_SendFrame( num_buf, msg_isr_tx_can.can_id | CAN_EXTENDED_FRAME_ID, msg_isr_tx_can.frm_type, msg_isr_tx_can.len, msg_isr_tx_can.data ); // передали сообщение контроллеру } } } }}
So, sended messages are in the queue ( I use FreeRTOS ).
May be influenced by a context switch?
Although it seems to me that this should lead only to further delay.
Best regards,
Sergey.
I don't see what happens in SendFrame(), but you are calling it always with the same num_buf=0. It could be that ISR disables interrupt for buf2 and calls SendFrame to fill buf0, which will fail in case buf0 is busy.
Hello, Kef.
Thanks for the answer, but it still does not understand.
I did interrupt levels of the ECT and CAN identical, there seems to be no more mistakes
ISR priority has nothing to do with sending CAN messages. Look for errors in your software.