Versatile LCD adapter board for K70 available in KIT form.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Versatile LCD adapter board for K70 available in KIT form.

828 Views
iafg
Contributor IV

The TWR-PIM-41WVGA is a complete turnkey Kit for the Freescale tower system which is meant to work with processors that drive a TFT directly such as Kinetis K70, PXD and Vybrid. This Kit includes the Future Electronics exclusive TWR-PIM module, a high quality NL8048HL11 WVGA (800×480) TFT LCD from NLT (NEC) and the appropriate SLAB (Small LCD Adapter Board) for this specific display.

 

See here for more detail and video:

http://futurefreescaleguy.wordpress.com/2012/05/10/twr-pim41wvga/

0 Kudos
2 Replies

498 Views
4boysdad
Contributor I

I need to drive a 7" 800x480 color high resolution LCD+TP.

 

Any suggestions as to how wire to J5 & J6 on the secondary tower board? It would be nice to only have one interface PCB or cable to LCD+TP. I don't LCD+TP are standardized enough for that.

 

Any ideas.

 

 

Thank you

0 Kudos

498 Views
iafg
Contributor IV

Just learned that there is a $99 discount applied to the web-price of  TWR-PIM-41WVGA  (WVGA LCD Kit for K70) .

That discount is ending today, but you can get a coupon if you attend the Future Electronics HMI Seminar (PEG+K70) series that is running now.


0 Kudos