AnsweredAssumed Answered

[CW3.1 S12A128] Can ANYBODY tell me that this works?

Question asked by MIKE YETSKO on Feb 23, 2006
Latest reply on Feb 23, 2006 by desroc01
I don't really know if this is a CW issue or a hardware issue with the part.  I'm using the CW3.1 SE that comes with the USB BDM pod to program a 9S12A128.
 
Has ANYBODY been able to make the memory display windows in the CW Debugger display updated FLASH page data?  I'm trying to debug routines that reprogram the flash at a 'switched in page', and CW won't update.  I can see the 'original' data in the flash if I go out to it's 'real' address (388000h in this case) but it never changes.
 
I've spent a week and a half chasing down issues associated with this, and at this point if I'm told it won't work I'll just have to move 'around' the issue.  I can't spend any more time on it.

Message Edited by Alban on 02-23-2006 02:38 PM

Outcomes