Can this combination of modules be made to compile, program and run the demo (sensor, LED's Touch, Shell etc..) that comes on the tower system using the P&E multilink universal debugger? I was able to do "Hello world" in CW and the LED flash in IAR. Both running from ram. The full tower demo is a bit more elusive with many compile errors.
I have a CW license and the IAR demo and would like to use both for this evaluation. My goal is to look at debug cycle time (edit, compile, program, run to edit time) for a full working application with the two tools and see if the MK60 and tools make sense for us for a new design.
Specific directions for this combination would be most apreciated.
James
Solved! Go to Solution.
Yes it works!
You have to change the libary path to 3.8 (even though the demo is located there).
James
Yes it works!
You have to change the libary path to 3.8 (even though the demo is located there).
James