I have started a new project and am adding files. I am getting an odd warning when I add any header (*.h) file.
"At least one file could not be added to the selected target"
The file shows up in the project tree, but can not be searched. If I search for a term in the file, it returns nothing. However, when I build, it knows the file is there. I defined the same thing in two seperate header files (ex. #define TEST_DEF 1) and it was caught by the tool when I built.
The access paths for where the files are located are correct.
Attempting to do a build, even if it fails, corrects the problem of not being able to search inside the files.