DALE RODDA

Bootloader and flash read protection

Discussion created by DALE RODDA on Apr 11, 2012
Latest reply on Apr 12, 2012 by kef

I am confused about protecting flash from being read. I have the bootloader from AN4379 up and working. I want to protect the flash from reading and I still need to use the backdoor key to verify the part was correctly programmed at the factory. I think I need to do the following

1. In the bootloader file Boot_loader_task.c

       Set the KEYEN and SEC bits using NVOPT_INIT.

       Set the NVBACKKEY to my key.

2. At this point I an not sure what I have to do. When the bootloader runs does it need to enter the key to be able load the application. Can I include the key the application? Is this the correct approach?

Outcomes