CW10.2 Build 120126 / P.E. 1.1.0.b1202-0629

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.2 Build 120126 / P.E. 1.1.0.b1202-0629

Jump to solution
934 Views
MichaelMiller
Contributor I

I can't believe that this hasn't been answered somewhere but for the life of me I can't find it.

 

How can I change the name of a Bean in Processor Expert. I have output pins generated as Bit1 when it is really a LED!

 

Thanks in Advance

 

Mike.

0 Kudos
1 Solution
826 Views
CrasyCat
Specialist III

Hello

 

  This can be done as follows:

     - Double click on the bean in the Project panel to open the Component Inspector for the bean.

     - Switch to Advanced or Expert mode on the top right side of the Component Inspector View.

       From there you should be able to change the Component Name.

 

CrasyCat

View solution in original post

0 Kudos
1 Reply
827 Views
CrasyCat
Specialist III

Hello

 

  This can be done as follows:

     - Double click on the bean in the Project panel to open the Component Inspector for the bean.

     - Switch to Advanced or Expert mode on the top right side of the Component Inspector View.

       From there you should be able to change the Component Name.

 

CrasyCat

0 Kudos