AnsweredAssumed Answered

Use different chip package

Question asked by Yvan BOURNE on Mar 20, 2012
Latest reply on Mar 22, 2012 by Yvan BOURNE

Hello,

 

I have a board with a K60512VLL100 (a 100 pins) and try to design a MQX project on it.

 

For my first tests, I used the demo projects from the TOWER (which contains a K60512VMD, a 144 pins).

 

But now, I have a problem with SPI2 : on the TOWER, the demo project run and output some signals on the SCLK pin, but on my board, nothing...

 

I think it's the chip header that I have to change in the MQX project. I find that "MK60N512VMD100.h" is used in the PSP, but there is no "MK60N512VLL100.h" available in  the CW10.1/10.2 and MQX 3.7/3.8 directories...

 

Have an ideas ?

 

Thanks,

Yvan

Outcomes