Hi every one
I have a TWR-MCF255X board and as you know this board has an accelerometer and a potentiometer. What I'm trying to do is develop a simple application just to start using this board because I'm new at freescale MCUs.
At the component inspector the configuration I choose is the following for the "A/D channels"
_________________________________________________________
- A/D channels 4
- Channel0
A/D channel (pin) AN0_PAN0
A/D channel (pin) signal ACCX
+ Mode select Single Ended
- Channel1
A/D channel (pin) AN1_PAN1
A/D channel (pin) signal ACCY
+ Mode select Single Ended
- Channel2
A/D channel (pin) AN2_PAN2
A/D channel (pin) signal ACCZ
+ Mode select Single Ended
- Channel3
A/D channel (pin) AN3_PAN3
A/D channel (pin) signal POT
+ Mode select Single Ended
_________________________________________________________
The problem comes because a warning appears at the column "description" for the channel 1, 2 and 3, the warning says "Warning: This channel is not included in the list of samples. The channel won't be measured" and when I try to put this channels in the subcategories "Sample1, Sample2 and Sample3" respectively in the category "Queue" it doesn't allow me to change the values to other different than 0 that is already there for default. If I put other number different than "0" and hit enter it automatically returns to "0"
I don't know what am I doing wrong. Can anyone help me please?
Thank you very much for helping!! Regards
Solved! Go to Solution.
Hi,
I have reproduced the problem using the plain CodeWarrior 10.2 and it disappeared when I installed the MCU 10.2 Update 1.0.0. Please install that update and it should be fixed. You can use the menu command Help > Install new software...
best regards
Petr Hradsky
Processor Expert Support Team
Hello,
make sure you enable the sample in the Queue settings.
See attached image.
Hope this helps,
BK
Hi all,
It seems i got the same problem using Processor expert for ADC.
I use following configuration:
Codewarrior 10.2 Special edition
MCF52233 Demo board.
I tried almost every possibility but still I cannot set in "Queue" settings
anything. All the time I have 0 value even when "Sample" is set to "Enabled".
In attachment screen with warning i'm getting.
I just started with Processor expert and I do not really know what am I doing wrong.
Hi,
I have reproduced the problem using the plain CodeWarrior 10.2 and it disappeared when I installed the MCU 10.2 Update 1.0.0. Please install that update and it should be fixed. You can use the menu command Help > Install new software...
best regards
Petr Hradsky
Processor Expert Support Team
hi,
thanks It works.