Hi every one
I have so many problems with cw10.2 by the configuration so that i was thinking to go back in cw10.1.
i mean they is a really big defference between both of them? if it is the case can some one please list them to me, or some usefull example? because if it is no that much i will move back to cw10.1 + (mqx 3.8 )
thx
br
wilson
See this blog article for some general information on what's new in CW 10.2. Other features worth mentioning are:
1) When displaying live, updated data in the debugger, you can now set the poll rate (it had been a fixed value)
2) Better support for debugging sleep mode states on the MCU
I would say that unless you updated CodeWarrior to get a particular feature or bug fix, and V 10.1 suits your needs, then stick with it.
---Tom