Hi
I am finding some problem in Boot ROM Location setting for p1012.
When i made setting boot ROM location to Local bus GPCM-16-bit ROM (default) Codeworrior Initializing fine and am able write and read from Dithers is working perfectly fine.
But when I changed boot ROM location to Local bus FCM-8-bit NAND flash small page (or any other mode) Codeworrior Initializing fails.(???).
I am fully confused that why its happening.
Please Help me.
Solved! Go to Solution.
Hi all i got the answer
When NAND boot is selected the processor will be able to complete its POR
sequence only if the NAND flash contains data with correct ECC.
From the POR sequence description provided in the P1021 QorIQ Integrated
Processor Reference Manual (4.5.2 Power-On Reset Sequence, step 8) you could
see that further progress is posible only after the FCM finishes loading the
pages from the NAND Flash device - else (for a blank NAND device) the POR
sequence stalls forever.IIn the described case it is required to select boot ROM location to Local
bus GPCM, connect CodeWarrior and program NAND flash. After that it will be
possible to change the ROM location to NAND.
Hi
I am finding some problem in Boot ROM Location setting for p1012.
When i made setting boot ROM location to Local bus GPCM-16-bit ROM (default) Codeworrior Initializing fine and am able write and read from DDR3 it is working perfectly fine.
But when I changed boot ROM location to Local bus FCM-8-bit NAND flash small page (or any other mode) Codeworrior Initializing fails.(???).
I am fully confused that why its happening.
Please Help me.
Hi all i got the answer
When NAND boot is selected the processor will be able to complete its POR
sequence only if the NAND flash contains data with correct ECC.
From the POR sequence description provided in the P1021 QorIQ Integrated
Processor Reference Manual (4.5.2 Power-On Reset Sequence, step 8) you could
see that further progress is posible only after the FCM finishes loading the
pages from the NAND Flash device - else (for a blank NAND device) the POR
sequence stalls forever.IIn the described case it is required to select boot ROM location to Local
bus GPCM, connect CodeWarrior and program NAND flash. After that it will be
possible to change the ROM location to NAND.
Thanks I may need to know that....
Can I ask what development board you are using?
Thanks R
For other, I'm trying to find if this is a popluar processor ... see blow
https://community.freescale.com/thread/109732
https://community.freescale.com/thread/109730
Hi Rick
Thanks. We are using P1020 RDB since we could nt get P1021 RDB and our target application (for our Product) is on P1012 processor.
Thanks for the reply
For others, you can actually buy this board, just type P1021RDB-PC into the search box on freescales web site. It seems that the website is out of date, however, this is a fairly new board and I have been informed by freescale that this will be fixed
Hi Rick
we are facing some problem when the processor NAND (small page) booting.
Actually through FCM mode we are able to boot p1012.
But our Design (FPGA and CPLD) register access done through( using chip selects LCS1 and LCS2 ) eLBC GPCM mode.
We are unable to write into these registers when the boot is NANd (FCM mode).
But we are able to write and read if we select SDCARD boot.
Are you aware of this problem.why NAND Boot has problem.
Is there any boot code modification required to change the mode from FCM to GPCM after the booting.