Hello,
My question is a little bit silly, but, when I'm debugging with CW10.2, I can't find how to display char array as C string.
Choices formats are Natural, Decimal, Hexadecimal, Binary and fractional, but ASCII seems to miss?
Hello,
I missed something huge, or it's a real lack?
Hi!
I'm not familiar with CW010... I'm using CW4.6 and CW6.3... in both cases, if I want to see the Array as String characters inside the Data Component, I set the format to "Symbolic"... That's not on your list, so I'll try NATURAL o DECIMAL...
Or you can view it inside the MEMORY component, just input the variable address or right-click on it inside the DATA component and then click on "Show Location"... there you can see it as string characters
If you're working with a paged memory model, remember to set the right page.
Hope it helps!
Hi,
Things doesn't seem to be so clear in CW10 than in classic IDE .