I'm sorry to postthis Message.
I have installed MQX 3.8 today, the default C++ demo works well without standard c++ libraries.
but I'd like to include some standard C++ libraries, such as <iostream>, <list>, etc.
i have added this to comiple option: "${MCUToolsBaseDir}/ColdFire_Support/ewl/EWL_C++/include"
and then i just add one line : #include <iostream>, and rebuild the project.
there were many errors happened:
undefined identifier 'wmemset' Dragon line 240 C/C++ problem
undefined identifier 'wmemmove' Dragon line 240 C/C++ problem
undefined identifier 'wmemcpy' Dragon line 242 C/C++ problem
undefined identifier 'wmemcmp' Dragon line 242 C/C++ problem
..........
what should i do next?
thank you all!
Hi autobio,
is there any progress with iostream ?
Start with mqx_cnfg.h file . Check these two : MQX_SUPPRESS_FILE_DEF , MQX_SUPPRESS_STDIO_MACROS.
There are many compilation defines which you could disable if you dont need them (_EWL_NO_IO in iostream as an example).
Regards,
MartinK
It's ok now, except the <iostream>.