Hi All,
I am trying to download a binary image using CW10.2 Beta and I am getting the following error. Any clues whats happenning. The following is the console output
fl::target -lc "LC for Simple Flash (1)"
fl::target -b 0x20000000 0x10000
fl::target -v off -l off
cmdwin::fl::device -d "FTFL_PFlash512" -o "128Kx32x1" -a 0x0 0x7ffff
cmdwin::fl::image -f "D:\\K60_Tower_Kit\\uTaskerV1_4-014.bin" -t "Auto Detect" -re on -r 0x0 0x7ffff -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Binary/Raw Format.
Performing target initialization ...
Downloading Flash Device Driver ...
Reading flash ID ...
Erasing Sector 0x00000000 to 0x000007FF
Erasing Sector 0x00000800 to 0x00000FFF
Erasing Sector 0x00001000 to 0x000017FF
Erasing Sector 0x00001800 to 0x00001FFF
Erasing Sector 0x00002000 to 0x000027FF
Erasing Sector 0x00002800 to 0x00002FFF
Erasing Sector 0x00003000 to 0x000037FF
Erasing Sector 0x00003800 to 0x00003FFF
Erasing Sector 0x00004000 to 0x000047FF
Erasing Sector 0x00004800 to 0x00004FFF
Erasing Sector 0x00005000 to 0x000057FF
Erasing Sector 0x00005800 to 0x00005FFF
Erasing Sector 0x00006000 to 0x000067FF
Erasing Sector 0x00006800 to 0x00006FFF
Erasing Sector 0x00007000 to 0x000077FF
Erasing Sector 0x00007800 to 0x00007FFF
Erasing Sector 0x00008000 to 0x000087FF
Erasing Sector 0x00008800 to 0x00008FFF
Erasing Sector 0x00009000 to 0x000097FF
Erasing Sector 0x00009800 to 0x00009FFF
Erasing Sector 0x0000A000 to 0x0000A7FF
Erasing Sector 0x0000A800 to 0x0000AFFF
Erasing Sector 0x0000B000 to 0x0000B7FF
Erasing Sector 0x0000B800 to 0x0000BFFF
Erasing Sector 0x0000C000 to 0x0000C7FF
Erasing Sector 0x0000C800 to 0x0000CFFF
Erasing Sector 0x0000D000 to 0x0000D7FF
Erasing Sector 0x0000D800 to 0x0000DFFF
Erasing Sector 0x0000E000 to 0x0000E7FF
Erasing Sector 0x0000E800 to 0x0000EFFF
Erasing Sector 0x0000F000 to 0x0000F7FF
Erasing Sector 0x0000F800 to 0x0000FFFF
Erasing Sector 0x00010000 to 0x000107FF
Erasing Sector 0x00010800 to 0x00010FFF
Erasing Sector 0x00011000 to 0x000117FF
Erasing Sector 0x00011800 to 0x00011FFF
Erasing Sector 0x00012000 to 0x000127FF
Erasing Sector 0x00012800 to 0x00012FFF
Erasing Sector 0x00013000 to 0x000137FF
Erasing Sector 0x00013800 to 0x00013FFF
Erasing Sector 0x00014000 to 0x000147FF
Erasing Sector 0x00014800 to 0x00014FFF
Erasing Sector 0x00015000 to 0x000157FF
Erasing Sector 0x00015800 to 0x00015FFF
Erasing Sector 0x00016000 to 0x000167FF
Erasing Sector 0x00016800 to 0x00016FFF
Erasing Sector 0x00017000 to 0x000177FF
Erasing Sector 0x00017800 to 0x00017FFF
Erasing Sector 0x00018000 to 0x000187FF
Erasing Sector 0x00018800 to 0x00018FFF
Erasing Sector 0x00019000 to 0x000197FF
Erasing Sector 0x00019800 to 0x00019FFF
Erasing Sector 0x0001A000 to 0x0001A7FF
Erasing Sector 0x0001A800 to 0x0001AFFF
Erasing Sector 0x0001B000 to 0x0001B7FF
Erasing Sector 0x0001B800 to 0x0001BFFF
Erasing Sector 0x0001C000 to 0x0001C7FF
Erasing ...
Erase Command Succeeded
cmdwin::fl::write
Beginning Operation ...
-------------------------
Using restricted address range 0x00000000 to 0x0007FFFF
Programming file D:\K60_Tower_Kit\uTaskerV1_4-014.bin
Auto-detection is successful.
File is of type Binary/Raw Format.
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Binary/Raw Format.
Downloading 0x0000EE98 bytes to be programmed at 0x00000000
Executing program ....
Error: Program failed. Flash driver reports the following error(s): Security area can not be programmed
Error: Program failed. Flash driver reports the following error(s): Security area can not be programmed
Thanks,
Mohsin
Can anyone from Freescale please help ?
Regards,
Mohsin
It seems that the flash is somehow secured on the chip. I did a search using the phrase "unsecure" on the Kinetis forum (since you are using a Kinetis part), and got the following results:
One of these forum threads might fit your situation and offer a solution.
---Tom
Hi Tom,
Thanks for your reply. I am not sure if its the same issue because I can debug individual programms by clicking the debug button. The issue comes up when loading a binary/hex file using "Flash File to Target".
There are some differences in how this is done using CW10.2 (which I am using) and using CW10.1 as in the following post
https://community.freescale.com/thread/103976
Thanks,
Mohsin
Depending upon how your CodeWarrior project is configured, when you click Debug the IDE might be downloading the program into RAM rather than flash, and so debugging works. From the communications trace, the IDE is talking to the part and erasing it. So, the evidence point to either the flash got secured somehow, or there's a secured region in the flash that you're trying to load the program in and the part balks at that.
Have you tried downloading any of the demo programs into flash successfully? That would tell you whether the part is secured, or if there's a secured area in flash.
Finally, since this problem seems to have appeared in v10.2, you might want to file an on-line service request to draw the engineers attention to this.
---Tom
Hi Tom,
Thanks for your reply. Yes, I am able to download programs to Flash normally. The issue is only when I use "Flash File to Target" option.
I think its time to file an on-line service request.
Regards,
Mohsin