Using HC908JL12 with CW 6.3 and XP. I see that ansif.lib is very much larger than ansii.lib, so I eliminated a few floating calculations and replaced ansif.lib by ansii.lib. Yet it appears that my code is the same size regardless which library I use. I do not know the structure of these libraries. I imagine it is possible for the linker to only link in the required routines but that kind of precision would be surprising. I am new to CW and may not be looking at the right numbers in the .map file. It lists many NOT USED PROCEDURES (and they are different) which I expect is (different) wasted space in Flash. In both .map files I have these identical sections:
TARGET SECTION
---------------------------------------------------------------------------------------------
Processor : Freescale HC08
Memory Model: SMALL
File Format : ELF\DWARF 2.0
Linker : SmartLinker V-5.0.37 Build 9279, Oct 7 2009
[...]
Summary of section sizes per section type:
READ_ONLY (R): 16FE (dec: 5886)
READ_WRITE (R/W): AB (dec: 171)
NO_INIT (N/I): 63 (dec: 99)
Isn't 5886 the majority of Flash? I know there are a few other contributions, but nothing that would change when the library is changed.
Are your libraries and linker that brilliant, or what am I missing?
Solved! Go to Solution.
cab wrote:I imagine it is possible for the linker to only link in the required routines but that kind of precision would be surprising.
Hi Cab,
The point of a library is that it is just a lirary of routines. You do not have to "check-out" the entire library, only the routines you need. Those NOT USED PROCEDURES are also not included in your flash image.
It looks like you are using under 6k of flash, so you should still have half of your flash empty.
The linker performs smart linking - in that it strips the symbols that are not actually used. This means that only the library routines that are used will be allocated to section .text. In order to see which exactly these routines are, check the object allocation section in the .map.file, looking for object files pertaining to the library, e.g.:
*********************************************************************************************
OBJECT-ALLOCATION SECTION
Name Module Addr hSize dSize Ref Section RLIB
---------------------------------------------------------------------------------------------
...
MODULE: -- RTSHC08.C.o (ansifs.lib) --
- PROCEDURES:
_PUSH_ARGS_L 2146 20 32 1 .text
_ENTER_BINARY_L 2166 16 22 2 .text
...
_FMUL 244D 7 7 1 .text
_FDIV 2454 7 7 1 .text
You will not see any of the not used procedures listed under the object allocation section.
If you sum up all the sizes (decimal: dSize) associated with section .text in the object allocation section, you obtain the size of .text as listed in the section allocation section of the map file.
cab wrote:I imagine it is possible for the linker to only link in the required routines but that kind of precision would be surprising.
Hi Cab,
The point of a library is that it is just a lirary of routines. You do not have to "check-out" the entire library, only the routines you need. Those NOT USED PROCEDURES are also not included in your flash image.
It looks like you are using under 6k of flash, so you should still have half of your flash empty.