CodeWarrior Power Architecture 10.1.1 and QorIQ Qonverge platform PSC9131RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Power Architecture 10.1.1 and QorIQ Qonverge platform PSC9131RDB

556 Views
NeenaB
Contributor I

I am using CodeWarrior Power Architecture 10.1.1 and i have connected PSC9131RDB. Actually in CodeWarrior Power Architecture 10.1.1, PSC9131 is not mentioned in the list of supported devices. So I selected P1010 as it contains single e500 core. With that configuration, i am able to bulid successfully. Bt when i tried 2 debug, at the end of debug session following error is getting displayed :

 

Failed to resume target process., CCSProtocolPlugin :  [CCS last error: USB open failure ]

 

How can i rectify this so that i can run my code on e500 core with PSC9131RDB using the IDE CodeWarrior Power Architecture 10.1.1?..

Labels (1)
0 Kudos
1 Reply

275 Views
J2MEJediMaster
Specialist I

Please do not cross-post your questiuon into other forums.

 

---Tom

0 Kudos