flashing problems via D-Bug12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flashing problems via D-Bug12

2,396 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Tue Apr 19, 2005 10:25 am    
 
Hello,

I try to flash an mc9s12hg256 via D-Bug12 monitor, but D-Bug12 gives everytime the same error: "Can't write target memory".
What could this mean?
To create the project I used the Codewizard from CodeWarrior, I tested several options without success.

Here is the s19-File:

 
Code:
S00E00004D6F6E69746F722E616273A5 S123C000FEC04BFDC049270E35ED31EC3169700434FB310326F2FEC04DEC31270BED311880 S123C0200A30700434F920F13D1EC0440203FFC047790011C6395B1086095A1207C215FBDE S123C040000320E500C06110FF0000C05BC06B0000C05B0000C05D0000C05DFFFF0000000B S110C0600010EFC6FF5B035B0120FE000033 S105FFFEC02914 S9030000FC 

 
I use the HCS12 T-Board from elektronik-laden.de

Any idea what I can do?

Greets
Posted: Tue Apr 19, 2005 12:11 pm 
 
Are there any switches on the device or instructions for programming the device that you have to follow? With my C32 sample board you had to put a switch in a certain position to program it and reset it then start the programming software.
Posted: Thu Apr 28, 2005 2:51 pm    
 
Hello everybody,
I've got exactly the same problem than elmachel.
I use an HCS12 Tboard from elektronic laden and codewarrior to assembly my S1.
Does somebody can help us?
Thank you
 
Posted: Fri Apr 29, 2005 8:06 am    
 
Hi,

the support from elektronikladen said without a BDMPod you can't programm the HCS12 effectivly. With D-Bug 12 you can only programm the RAM or the EEPROM but not the Flash. So you need a BDMPod or you configure the CodeWarrior to create s19 files for the RAM or EEPROM, but I don't know the configuiration.
I bought therefore the ComPOD12.

greetz

Posted: Fri Apr 29, 2005 8:47 am    

Hello,
do you manage with the compod to program your flash ?
Is it easy?
How does it work?
Waiting for your response,Bye

Posted: Sat Apr 30, 2005 4:48 am

Hello,

yes now I can programm the flash, it is quite easy. If you buy the Compod from elektronikladen there is a software with it, called Starprog. With this software you can erase/programm the controller. You are able to decide between programming in Flash or EEPROM.

buy

Posted: Sat Apr 30, 2005 3:58 pm    

If you can't afford to buy one build a TBDML insted, it will program/debug any S12 using the free Codewarrior software. You can get the PCB in our online store.


Labels (1)
0 Kudos
0 Replies