AnsweredAssumed Answered

K60N512 not booting after 30.07 bootloader update

Question asked by Nathan Ransom on Dec 22, 2011
Latest reply on Jan 2, 2012 by Martin Honig

I was attempting to run a sample project for MQX, and was required to download the latest updates for Codewarrior, which then required I update to the 30.07 bootloader for my tower board.  The update was able to succeed both within Codewarrior and through the PEMicro tool, but I can only boot into the bootloader programming mode.  When attempting to boot regularly nothing appears on the PC USB port so I cannot connect using the debugger or any other tool to attempt to program.  Not sure if something else was accidentally overwritten and needs to be reflashed?  Thanks for the help.

Outcomes