Hello
I have a problem with CW with 10.1 MQX 3.7 on Win 7 64bit. The same project is run on Win XP and everything is fine. The programonly with blinking LEDs and sends data to the UART. Under Wn 7 64bit on TWRK60N512 only LED blinking but does not send data to the UART. I have the same settings as USER_CONFIG under Win XP. Under Win 7 64bit I logged in as administrator and CW is installed to "C: \ Programs \ ..." not "C: \ Program Files \". I installed the same "PATCH" on both Win. I'm trying to "Build Project" "Build All" does not help anything. As would be noticed a change in "USER_CONFIG". Everything is the same, except for Windows(CW location C: \). We do not know how to fix the problem.
Please help.
Thank you very much for your advice.
Cerma
Cerma,
Sorry that I didn't see any reply post to your problem since Dec.
Did you ever got your problem resolved?
We have 10.2 and MqX 3.8 now.
Make sure to manually run the batch file in MQX3.8 to install the the Kernal Aware Debugger tools into 10.2.
MQXdirectory .... \tools\codewarrior_extensions\CW MCU v10.2 \install_cw10_plugin.bat “C:\Freescale\cw mcu v10.2”
hy