Dear all,
I am trying to use my CodeWarrior 10.1 with the license that I own and that I previously used on a previous pc with Win XP.
I have plugged the USB Dongle and it autoinstalled correctly, without any problems. After that, I run the FlexLM program and found that I can see the FlexID in the screen (lmtools.exe --> System Settings --> FLEXID --> x-abcdefgh).
I have copied the license.dat file that I own to the CodeWarrior path, C:\Program Files (x86)\Freescale\CW MCU v10.1\MCU, in which there used to be the 30 day free license.
After that I configured in the lmtools the following service:
ServiceName: CodeWarrior 10
Parth to the license file: C:\Program Files (x86)\Freescale\CW MCU v10.1\MCU\license.dat
I also have the paths for teh tool and log files, but they are not related to the problem.
I accepted (tick) the "Use Services" option and the "Start Server at Power Up" option.
After that I rebooted my computer and the run the CodeWarrior, but it says the following:
What am I doing wrong?
Thanks for your help.
Best regards.
See if these forum threads can help:
https://community.freescale.com/message/100044#100044
https://community.freescale.com/message/98688#98688
---Tom