Using shell examples with terminal I/o

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using shell examples with terminal I/o

Jump to solution
623 Views
ronysha
Contributor II

I am using IAR. In order to use the terminal I/o of the tool instead of external terminal e.g.. pemicro I have to do some settings.

I am able to  force the printf and gets functions to use the terminal I/O (by commenting the #define printf of fio.h).

But shell.c printf and similar commands still try to access the uart. How can I force them to approach the terminal I/o too?

Thanks

 

Labels (1)
Tags (1)
0 Kudos
1 Solution
294 Views
c0170
Senior Contributor III

hi ronysha,

 

there is IODEBUG feature in MQX 3.8 which uses ide terminal. If it is enabled in user_config.h and board.h selected as default, everything is printed to the i/o terminal.

 

Regards,

MartinK

View solution in original post

0 Kudos
1 Reply
295 Views
c0170
Senior Contributor III

hi ronysha,

 

there is IODEBUG feature in MQX 3.8 which uses ide terminal. If it is enabled in user_config.h and board.h selected as default, everything is printed to the i/o terminal.

 

Regards,

MartinK

0 Kudos