Hello!
I write my application and tested it inside internal RAM. Now I wanna flash it to use it as a stand alone application.
Therefore I changed the debug configuration from MK60N512VMD100_INTERNAL_RAM to MK60N512VMD100_INTERNAL_FLASH, but it has no effect.
With the internal Flash configuration I can debug my program as before. But after a reset or after power up my application doesn t run.
Using the flash might be more complicated than I expect.
So what must I do to get my program into flash?
I also try to use the simple flash programmer that is part of Codewarrior, but I alway get error messages when I try to use it.
I use the TWR K60 Tower and CodeWarrior 10.1
May Thanks
Ulf
Please do not cross post your question into other forums. I have answered it elswhere.
---Tom