i.MX8M [Coral Dev] Flashing rootfs > 4GB yields corrupt eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M [Coral Dev] Flashing rootfs > 4GB yields corrupt eMMC

1,139 Views
petervdperk
NXP Employee
NXP Employee

Flashing a rootfs > 4GB to the Coral dev eMMC yields a corrupted rootfs.

The u-boot version runing on the Coral dev board is U-Boot 2017.03.3 (Nov 08 2019 - 22:29:30 +0000)

I've tried flashing using the Google fastboot and uuu from (GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. ).

Both yield a corrupted rootfs.

 

To reproduce this simply flash an image > 4GB to the rootfs partition.
FB: flash -raw2sparse rootfs rootfs_arm64.img

 

My assumption would be that somewhere an overflow occurs which overwrites the eMMC therefore corrupting the rootfs.

Labels (1)
0 Kudos
0 Replies