MX8-DSI-OLED1 ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8-DSI-OLED1 ERROR

1,072 Views
blackhuang
Contributor I

Hi,
I have recently purchased imx8mmevk board.
Now I've got L4.14.98_2.0.0_ga_image_MX8MMEVK in board,and there is a display on the 'MX8-DSI-OLED1'board.I did it according to the manual,but the error occured.the error  followed:

u-boot=>setenv fdt_file fsl-imx8mq-evk-dcss-rm67191.dtb

u-boot=> run bootcmd

switch to partitions #0, OK

mmc1(part 0) is current device

** Unable to read file boot.scr **

23163392 bytes read in 283 ms (78.1 MiB/s)

Booting from mmc ...

** Unable to read file fsl-imx8mq-evk-dcss-rm67191.dtb **

WARN: Cannot load the DT

 

 

 

thanks.

Labels (1)
0 Kudos
0 Replies