Thank you in advance for your help.
Q_1: Is LPDDR4 located in EVK discontinued?
Unable to find datasheet for MT53B768M32D4NQ-062 WT:B on Micron site.
Q_2 :If MT53B768M32D4NQ-062 WT:B is discontinued, can I receive the data sheet for the replacement product MT53B768M32D4DT-062 AIT:B?
Q:3 : Is it okay to use MT53B768M32D4DT-062 AIT:B instead of MT53B768M32D4NQ-062 WT:B?
These two memory devices only have a difference in SMD.
Please reply.
Hi,
See below, please!
Q_1: Is LPDDR4 located in EVK discontinued?
No, it is not. i.MX8MQ supports LPDDR4.
Q_2 :If MT53B768M32D4NQ-062 WT:B is discontinued, can I receive the data sheet for the replacement product MT53B768M32D4DT-062 AIT:B?
yes, you can. MT53B768M32D4DT-062 AIT:B has been used on i.MX8QM-MEK board, so you can also use it on iMX8MQ board.
Q:3 : Is it okay to use MT53B768M32D4DT-062 AIT:B instead of MT53B768M32D4NQ-062 WT:B?
Yes, it is.
Have a nice day!
B.R,
weidong
I have confirmed that MT53B768M32D4DT-062 AIT has been discontinued.
Can MT53E768M32D4DT-046 be used as a replacement?