imx8mp lite chromium takes a log time to start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp lite chromium takes a log time to start

1,415 Views
diegoperez
Contributor II

Hi,

On our imx8mp board we mount the complete imx8mp with NPU VPU and also the imx8mp lite without NPU or VPU. I have observed that when running chromium in the imx8mp lite version it takes a long time for it to appear on the screen, about 2 minutes compared to a few seconds in the full imx8mp version. We are currently using BSP version 6.1.36. I put the log when running Chromium with the verbose option, I send a file with the complete startup and I put here the first place where it stops for 50 seconds:

[4407:4427:0418/124211.023550:VERBOSE1:tls_client_handshaker.cc(508)] Client: handshake finished

[4376:4402:0418/124241.948777:VERBOSE1:v4l2_device.cc(2516)] empty.... Try Multi-plane
[4376:4402:0418/124241.953920:VERBOSE1:gpu_video_decode_accelerator_factory.cc(113)] GetDecoderCapabilities(): Capabilities empty, querying again...

[4407:4427:0418/124301.075844:VERBOSE1:network_delegate.cc(34)] NetworkDelegate::NotifyBeforeURLRequest: https://update.googleapis.com/service/update2/json?cup2key=11:zkseNLX3qMugXYVo-EWX82gDYYInad9IfWIaP8...
[4407:4427:0418/124301.076751:VERBOSE1:network_delegate.cc(34)] NetworkDelegate::NotifyBeforeURLRequest: https://doh.opendns.com/dns-query?dns=AAABAAABAAAAAAABBnVwZGF0ZQpnb29nbGVhcGlzA2NvbQAAAQABAAApEAAAAA...
[4376:4376:0418/124301.350876:VERBOSE1:request_sender.cc(181)] Request completed from url: https://update.googleapis.com/service/update2/json?cup2key=11:zkseNLX3qMugXYVo-EWX82gDYYInad9IfWIaP8...
[4376:4376:0418/124301.355517:VERBOSE1:component_updater_service.cc(455)] Update completed with error 0

Thanks and best regards.

 

0 Kudos
Reply
0 Replies