imx kernel fails to load

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx kernel fails to load

797 次查看
solve_this
Contributor II

mmc0(part 0) is current device
Scanning mmc 0:1...
Failed to load '/'
MMC: no card present
optee optee: OP-TEE api uid mismatch
Unable to open OP-TEE session (err=-19)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
switch to partitions #0, OK
mmc0(part 0) is current device
Failed to load 'boot.scr'
32262656 bytes read in 192 ms (160.2 MiB/s)
Booting from mmc ...
61388 bytes read in 15 ms (3.9 MiB/s)
792 bytes read in 4 ms (193.4 KiB/s)
Working FDT set to 43000000
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Working FDT set to 43000000
clk usb1_phy_root_clk already disabled
clk usb2_phy_root_clk already disabled
Using Device Tree in place at 0000000043000000, end 0000000043012fff
Working FDT set to 43000000

0 项奖励
回复
0 回复数