i.MX53 preinstalled ubuntu image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX53 preinstalled ubuntu image

1,192 Views
azap
Contributor I

I have an old board i.MX53 and would like to start using it as a light web server.  However, I can't find any preinstalled images on the web anymore. Seems like everything is obsolete.  It's a bad luck I erased the demo image

Previously, I was able to download lots of preinstalled images by simply burning them to SD card.  Today I was only able to find the following image:

https://old-releases.ubuntu.com/releases/precise/ubuntu-12.04-preinstalled-desktop-armhf+mx5.img.gz

Unfortunately, mouse and keyboard do not work with this one, and yeah, I know that the mux may not be right in the kernel.  However, even though I just need a network, there is no way I can configure the network without any basic input.

Can someone please send me the standard MX53_QSB_UBUNTU_SD_DEMO_IMAGE image, which seems not available anymore?

I would also appreciate if someone has a link to ubuntu preinstalled server setup for MX53. I am pretty sure it existed before, but any operational image should be fine.

Thanks

0 Kudos
Reply
1 Reply

1,143 Views
azap
Contributor I

Anyone at NXP can help me get the old image?

0 Kudos
Reply