I have an old board i.MX53 and would like to start using it as a light web server. However, I can't find any preinstalled images on the web anymore. Seems like everything is obsolete. It's a bad luck I erased the demo image
Previously, I was able to download lots of preinstalled images by simply burning them to SD card. Today I was only able to find the following image:
https://old-releases.ubuntu.com/releases/precise/ubuntu-12.04-preinstalled-desktop-armhf+mx5.img.gz
Unfortunately, mouse and keyboard do not work with this one, and yeah, I know that the mux may not be right in the kernel. However, even though I just need a network, there is no way I can configure the network without any basic input.
Can someone please send me the standard MX53_QSB_UBUNTU_SD_DEMO_IMAGE image, which seems not available anymore?
I would also appreciate if someone has a link to ubuntu preinstalled server setup for MX53. I am pretty sure it existed before, but any operational image should be fine.
Thanks
Anyone at NXP can help me get the old image?