how to integrate the external Wi-Fi BT module on the IMX8QuadMax MEK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to integrate the external Wi-Fi BT module on the IMX8QuadMax MEK

1,007 次查看
K_Varun
Contributor III

Dear Community,

I have installed the following Wi-Fi BT module in the slot of my i.MX8QM MEK board and flashed Auto 13 OS.

Wi -Fi BT module link : https://in.element14.com/laird/st60-2230c-u/bt-wifi-module-2-4-2-495-5-15/dp/3407266

I am facing some issues and need guidance:

  1. I cannot see any local wi-fi or Bluetooth devices on the settings page after flashing the OS.
  2. How can I check if the module is functioning correctly?
  3. Is this module compatible with the IMX8QM-MEK board?
  4. What changes are required to make the module work?

Your support on this matter would be greatly appreciated.

Regards,
K. Varun

标记 (1)
0 项奖励
回复
1 回复

961 次查看
K_Varun
Contributor III

Dear Community,

Can someone please reply on this query. It helps me a lot.

Regards 

K Varun

0 项奖励
回复