how can i build one trusted application for NXP 8MPLUS BB LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i build one trusted application for NXP 8MPLUS BB LPDDR4

705件の閲覧回数
Avi2
Contributor I

Hi All,
I have built the core minimal image of yocto build for my NXP 8MPLUS BB board following this guide https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 
i have checked that OPTEE is present in my build now i want to create one trusted application for the same please guide me how can i do that either by yocto or any other way

Thank you

0 件の賞賛
返信
3 返答(返信)

681件の閲覧回数
AshutoshNama
Contributor III

Hi Avi, Set Up Your Development Environment.

Ensure your Yocto build environment is properly configured and that OP-TEE is included in your image. 

Install the required tools for developing Trusted Applications:
Toolchains: OP-TEE uses arm -none-eabi-gcc for building TAs.
Repositories: Clone the OP-TEE repositories, including optee_os, optee_client, and optee_examples from OP-TEE Github.
Create a new TA project directory under optee_examples or similar.
Write your trusted application code.
Create a new TA project directory under optee_examples or similar.

Build the TA using the OP-TEE build system:

Navigate to your Yocto build environment.
Integrate the TA into the Yocto recipe:
After building, you will have the .ta binary in the output folder.
Deploy the TA by copying it to the /lib/optee_armtz/ directory on your target board. Ensure that it matches the UUID defined in your application.
Test and Debug Your TA.

 

I hope the above instructions helped you, feel free to write & ask me any questions!

BR,
Ashutosh Nama.

0 件の賞賛
返信

689件の閲覧回数
Robert344Humphries
Contributor II

Hello!

To create a Trusted Application (TA) for OP-TEE on your NXP 8MPLUS BB board, set up your development environment, create the TA directory structure, write the TA code with the necessary entry points, build the TA using the OP-TEE TA-devkit, and deploy the TA binary to your target device. 

0 件の賞賛
返信

685件の閲覧回数
Robert344Humphries
Contributor II

I hope this helps!

Best Regards,

Robert

MyACI

0 件の賞賛
返信