TIOCSRS485 no longer works with Linux v6.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TIOCSRS485 no longer works with Linux v6.1

673 Views
jeff06
Contributor II

Hello,
For a hardware target using an imx6ULL processor, I am switching from linux v4.14 to linux v6.1.
It's starting to work but I'm encountering a blocking problem with the management of Uarts in RS485 mode.
On initialisation with the function "ioctl(fd,TIOCSRS485, &rs485conf);" I get the error "Inappropriate ioctl for device".

what do I have to do for the "TIOCSRS485 " command to be taken into account as in linux v4.14 ?

thank you for your help.

0 Kudos
Reply
0 Replies