Looking for yocto build recipe for dtls enc/dec on gstreamer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for yocto build recipe for dtls enc/dec on gstreamer

Jump to solution
2,618 Views
Anton_K
Contributor III

Hello! I'm looking for gstreamer-plugins-bad package configuration to have dtls ON for gstreamer. I'm building custom yocto project distro for specific board.
To enable DTLS on gstreamer-plugins-bad I suppose I have to enable on my local.conf:

...
MAGE_INSTALL:append = " gstreamer1.0-plugins-bad"
...

also on the recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_%.bbappend added:

...
PACKAGECONFIG:append = " dtls"
...

During build it's OK, but on the destination device with yocto NO dtlsenc/dtlsdec occur. I can check it with 

gst-inspect-1.0 |grep dtls


Platform: VAR-SOM-i.MX8X
OS version: poky
Kernel: Kirkstone-5.15.2

Can someone support me on this question? And how to predict which packages need to install for another package configuration, does that dependencies described somewhere?
Thanks in advance, Anton Kalistratov

0 Kudos
Reply
1 Solution
2,486 Views
L_VPS
Contributor I

Hi , I've came across the same error and I found a workaround:

In my gstreamer1.0-plugins-bad recipe i see the following:

PACKAGECONFIG_REMOVE ?= " \
dtls vulkan \
${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '', 'gl', d)} \
"
PACKAGECONFIG:remove = "${PACKAGECONFIG_REMOVE}"

Which seems to forbid to build the dtls elements.
In a .bbappend file I therefore altered the PACKAGECONFIG_REMOVE variable.

Surely there is a reason why dtls is explicitly disabled but it works for me...

I also had another issue with the element where it couldn't find some srtp element, so I also added srtp to the PACKAGECONFIG which again failed to run as it missed the libsrtp.so on the image.

The reason I found is that PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp" lists libsrtp in the wrong place.
Should be PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp,libsrtp" so libsrtp is also listed as a RDEPENDS.

 

Finally, my gstreamer1.0-plugins-bad_%.bbappend:

PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp,libsrtp"

PACKAGECONFIG_REMOVE = " \
vulkan \
${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '', 'gl', d)} \
"

PACKAGECONFIG:mx8mp-nxp-bsp += "dtls srtp"

(Edit: formatting)
(Edit 26. Sept.: The PACKAGECONFIG was actually wrong as we saw, fixed it)

View solution in original post

2 Replies
2,487 Views
L_VPS
Contributor I

Hi , I've came across the same error and I found a workaround:

In my gstreamer1.0-plugins-bad recipe i see the following:

PACKAGECONFIG_REMOVE ?= " \
dtls vulkan \
${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '', 'gl', d)} \
"
PACKAGECONFIG:remove = "${PACKAGECONFIG_REMOVE}"

Which seems to forbid to build the dtls elements.
In a .bbappend file I therefore altered the PACKAGECONFIG_REMOVE variable.

Surely there is a reason why dtls is explicitly disabled but it works for me...

I also had another issue with the element where it couldn't find some srtp element, so I also added srtp to the PACKAGECONFIG which again failed to run as it missed the libsrtp.so on the image.

The reason I found is that PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp" lists libsrtp in the wrong place.
Should be PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp,libsrtp" so libsrtp is also listed as a RDEPENDS.

 

Finally, my gstreamer1.0-plugins-bad_%.bbappend:

PACKAGECONFIG[srtp] = "-Dsrtp=enabled,-Dsrtp=disabled,libsrtp,libsrtp"

PACKAGECONFIG_REMOVE = " \
vulkan \
${@bb.utils.contains('DISTRO_FEATURES', 'wayland', '', 'gl', d)} \
"

PACKAGECONFIG:mx8mp-nxp-bsp += "dtls srtp"

(Edit: formatting)
(Edit 26. Sept.: The PACKAGECONFIG was actually wrong as we saw, fixed it)

2,581 Views
Anton_K
Contributor III

UPD. Also after build package config info returns no dtls:

 

$ bitbake -e gstreamer1.0-plugins-bad | grep PACKAGECONFIG=
PACKAGECONFIG="     orc     bluez      x11     wayland     gl     bz2 closedcaption curl dash  hls openssl sbc smoothstreaming     sndfile ttml uvch264 webp     rsvg  kms tinycompress gcrypt openjpeg opusparse rtmp sctp srt srtp tinyalsa v4l2codecs webrtc webrtcdsp zbar"

 

0 Kudos
Reply