Issue with flashing image to the nitrogen 8m mini sbc board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue with flashing image to the nitrogen 8m mini sbc board?

1,838 Views
tech04
Contributor I

Hi,

We have downloaded the pre-built yocto image 20231206-boundary-image-multimedia-full-nitrogen8mm-kirkstone.wic.gz  from Ezurio and flashed that image to the Nitrogen 8M Mini SBC board with the help of Balena etcher and dd utility on linux machine after giving ums 0 mmc 0:0 command in u-boot mode, board is booting up but not completely booting we are encountering errors that Unable to read file uEnv.txt **
** Unable to read file /imx8mq-nitrogen8m_som.dtb **
!!!! Error loading /imx8mq-nitrogen8m_som.dtb,  and after that we placed the uEnv.txt and   imx8mq-nitrogen8m_som.dtb files in boot and rebooted the board and kernel is starting up logs were floating but complete booting is not happening again we are seeing errors ,do we need to do any further changes to flash the image to board or what? could you please help me on the.

the following images shows the error we are encountering.please have a look on that.

0 Kudos
Reply
1 Reply

224 Views
gary_bisson
Senior Contributor III

Hi,

Something is wrong with the U-Boot environment OR you are the wrong platform.

Please take a picture of your platform.

Also, support for Ezurio platform is better through support@ezurio.com rather than NXP forum.

Regards,

0 Kudos
Reply