IMX95 Wont Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX95 Wont Boot

1,473 次查看
LewisEll
Contributor I

I have been attempting to boot the IMX95 board through its SD card, although the Boot Configuration is correct (1011) as suggested by the documentation sent with the board, it still does not output any display to he screen.

 

First I attempted with a manually bitbaked image (including podman-flutter), and as per the documentation, I flashed the SD card (128GB) with the command's on the official 'i.MX Yocto Project User's Guide':

$ zstdcat imx-image-full-imx95-19x19-lpddr5-evk.rootfs.wic.zst > imx2-image-full-imx95-19x19-lpddr5-evk.rootfs.wic

$ sudo dd if=imx2-image-full-imx95-19x19-lpddr5-evk.rootfs.wic of=/dev/mmcblk0 bs=1M conv=fsync

 

The action successfully carries out

10048+1 records in
10048+1 records out
10536514560 bytes (11 GB, 9.8 GiB) copied, 176.798 s, 59.6 MB/s

And both Boot and Root Partitions are made.

 

After inserting the flashed SD card with the relevant files into the IMX95 device, turning it on the led's light up green, but no display is output to the connected monitor througn HDMI (I have tested the cable with another device, not an issue with monitor or cable)

 

I connected my external laptop to the debug port to attempt resolving this issue using minicom:

#####################  Power Mode Switch Task ####################

   Build Time: Aug 26 2024--11:10:50  
   Core Clock: 800000000Hz  

Select the desired operation  

Press  A to enter: Normal RUN mode
Press  B to enter: WAIT mode
Press  C to enter: STOP mode
Press  D to enter: SUSPEND mode
Press  P to suspend A55 core
Press  W to wakeup A55 core

Waiting for power mode select..

Handle Peer Core Linkup

(End)

Once I select 'A' for 'Normal RUN mode' it seems to be an endless loop of just printing the same selections right after, and not actually carrying out the request to the Board.

 

I have carried out the process of re-flashing the SD card with the officially supplied image on the IMX Website (LF_v6.6.36-2.1.0_images_IMX95EVK.zip)

$ zstdcat imx-image-full-imx95evk.wic | sudo dd of=/dev/mmcblk0 bs=1M conv=fsync

But still no display output to the monitor, and minicom has the same issue:
Task 1 is working now                                                                                                       
                                                                                                                           
####################  Power Mode Switch Task ####################

   Build Time: Aug 26 2024--11:10:50  
   Core Clock: 800000000Hz  

Select the desired operation  

Press  A to enter: Normal RUN mode
Press  B to enter: WAIT mode
Press  C to enter: STOP mode
Press  D to enter: SUSPEND mode
Press  P to suspend A55 core
Press  W to wakeup A55 core

Waiting for power mode select..

A ## (local echo enabled)
####################  Power Mode Switch Task ####################

   Build Time: Aug 26 2024--11:10:50  
   Core Clock: 800000000Hz  

Select the desired operation  

Press  A to enter: Normal RUN mode
Press  B to enter: WAIT mode
Press  C to enter: STOP mode
Press  D to enter: SUSPEND mode
Press  P to suspend A55 core
Press  W to wakeup A55 core

Waiting for power mode select..

 

I am running out of possible solutions and would really appreciate any help with this if anybody has any ideas.

0 项奖励
回复
0 回复数