[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

843件の閲覧回数
Kunyang_Fan
Contributor II

Hi  Expert, 

I have a "i.MAX 8M PLUS EVK" and use the yocto code base "imx-yocto-bsp_5.10.72-2.2.0" and the image building command as below: 

$  repo init -u git://source.codeaurora.org/external/imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0_harpoon.xml

$   DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build 

$ bitbake imx-image-multimedia

After flashing to SD card and booting, there is only can device "can0" as below picture

Is anyway to enable the secondary can1? Rebuild the image or some commands need to input ?

Thanks,

only_can0_on_8mp_evk.png

タグ(1)
0 件の賞賛
0 返答(返信)