[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

1,175 次查看
Kunyang_Fan
Contributor II

Hi  Expert, 

I have a "i.MAX 8M PLUS EVK" and use the yocto code base "imx-yocto-bsp_5.10.72-2.2.0" and the image building command as below: 

$  repo init -u git://source.codeaurora.org/external/imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0_harpoon.xml

$   DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build 

$ bitbake imx-image-multimedia

After flashing to SD card and booting, there is only can device "can0" as below picture

Is anyway to enable the secondary can1? Rebuild the image or some commands need to input ?

Thanks,

only_can0_on_8mp_evk.png

标记 (1)
0 项奖励
回复
0 回复数