[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[I.MX 8M PLUS EVK] How to enable secondary CAN device "can1"

847 Views
Kunyang_Fan
Contributor II

Hi  Expert, 

I have a "i.MAX 8M PLUS EVK" and use the yocto code base "imx-yocto-bsp_5.10.72-2.2.0" and the image building command as below: 

$  repo init -u git://source.codeaurora.org/external/imx/imx-manifest.git -b imx-linux-hardknott -m imx-5.10.72-2.2.0_harpoon.xml

$   DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh -b build 

$ bitbake imx-image-multimedia

After flashing to SD card and booting, there is only can device "can0" as below picture

Is anyway to enable the secondary can1? Rebuild the image or some commands need to input ?

Thanks,

only_can0_on_8mp_evk.png

Tags (1)
0 Kudos
0 Replies