How to Boot i.MX6 Quad/DualLite from SATA (SSD)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Boot i.MX6 Quad/DualLite from SATA (SSD)?

583 次查看
felo05
Contributor I

Hello,

I am working with an i.MX6 Quad/DualLite system and need to boot from an SSD connected via SATA. Currently, I can successfully boot from SD card and eMMC using the following DIP switch configurations:

SD Card Boot: 1-4-6-8 ON

eMMC Boot: 1-2-4-5-6-8 ON

However, I could not find the correct DIP switch combination for SATA (SSD) boot.

Here are the details of my system:

Processor: ARMv7 (Freescale i.MX6 Quad/DualLite)

Bootloader: Not explicitly defined, but I assume U-Boot is used

Current Behavior: The SSD is detected in Linux (lsblk and fdisk -l show it), but I cannot boot from it

Requirement: I need the correct DIP switch configuration and any additional steps required to enable booting from SATA

Could you provide guidance on:

The correct DIP switch settings for SATA boot.

Whether I need to flash U-Boot or any other firmware on the SSD.

Any additional configuration steps (e.g., setting U-Boot environment variables).

Any help would be greatly appreciated. Thank you!

标记 (1)
0 项奖励
回复
0 回复数