How to Boot i.MX6 Quad/DualLite from SATA (SSD)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Boot i.MX6 Quad/DualLite from SATA (SSD)?

298件の閲覧回数
felo05
Contributor I

Hello,

I am working with an i.MX6 Quad/DualLite system and need to boot from an SSD connected via SATA. Currently, I can successfully boot from SD card and eMMC using the following DIP switch configurations:

  • SD Card Boot: 1-4-6-8 ON
  • eMMC Boot: 1-2-4-5-6-8 ON

However, I could not find the correct DIP switch combination for SATA (SSD) boot.

Here are the details of my system:

  • Processor: ARMv7 (Freescale i.MX6 Quad/DualLite)
  • Bootloader: U-Boot
  • Current Behavior: The SSD is detected in Linux (lsblk and fdisk -l show it), but I cannot boot from it
  • Requirement: I need the correct DIP switch configuration and any additional steps required to enable booting from SATA

Could you provide guidance on:

  1. The correct DIP switch settings for SATA boot.
  2. Whether I need to flash U-Boot or any other firmware on the SSD.
  3. Any additional configuration steps (e.g., setting U-Boot environment variables).

Any help would be greatly appreciated. Thank you!

0 件の賞賛
返信
0 返答(返信)