Enable tethering on eth0 Android 10 - imx8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enable tethering on eth0 Android 10 - imx8

2,679 Views
mauriciorodrigu
Contributor II

Hi all,

We're trying to replicate the tethering from wifi hotspot to ethernet interface, but without success. In the past it was enough to add some common commands on iptables and it would work, right know it seems like it need something more. We're on imx8m and still no luck. Ethernet drivers and connection is ok. We just can't enable tethering on this interface from wwan0.

Has any one been able to do it?

Thanks in advance.

0 Kudos
Reply
2 Replies

1,793 Views
Igor
Contributor III

Hi Mauricio,
I have the same problem: I should enable GSM modem and Eth0 interface simultaneously and enable tethering. Can you give some advice?
Thank you,

 

igor

0 Kudos
Reply

2,612 Views
mauriciorodrigu
Contributor II

We have managed to achieve the tethering on the Eth0 interface,based on this solution : https://gitlab.edgecenter.io/b3399g/android-bsp/-/commit/e76f3f86ff3daf4cdc185121c7d082994b9317f9.

It now works.

0 Kudos
Reply