Enable tethering on eth0 Android 10 - imx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable tethering on eth0 Android 10 - imx8

2,725件の閲覧回数
mauriciorodrigu
Contributor II

Hi all,

We're trying to replicate the tethering from wifi hotspot to ethernet interface, but without success. In the past it was enough to add some common commands on iptables and it would work, right know it seems like it need something more. We're on imx8m and still no luck. Ethernet drivers and connection is ok. We just can't enable tethering on this interface from wwan0.

Has any one been able to do it?

Thanks in advance.

0 件の賞賛
返信
2 返答(返信)

1,839件の閲覧回数
Igor
Contributor III

Hi Mauricio,
I have the same problem: I should enable GSM modem and Eth0 interface simultaneously and enable tethering. Can you give some advice?
Thank you,

 

igor

0 件の賞賛
返信

2,658件の閲覧回数
mauriciorodrigu
Contributor II

We have managed to achieve the tethering on the Eth0 interface,based on this solution : https://gitlab.edgecenter.io/b3399g/android-bsp/-/commit/e76f3f86ff3daf4cdc185121c7d082994b9317f9.

It now works.

0 件の賞賛
返信