Connect Wi-Fi on the board i.MX8M Plus Evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect Wi-Fi on the board i.MX8M Plus Evk

4,222 Views
nikkiboss
Contributor I

Hi All,

I try to bring the Wi-Fi on IMX8M Plus, using Azurewave CM276 M.2 card.

My chip version i.MX 8M Plus Evk is A1.

I uploaded the image L5.4.70-2.3.0 imx-image-full. 

I execute "modprobe moal mod_para=nxp/wifi_mod_para.conf".

If I execute "wpa_supplicant -d -B -i mlan0 -c /etc/wpa_supplicant.conf -Dnl80211", I get "mlan0: Unsupported driver 'n180211'".

What should I do next? Сan anyone write step by step please?

Tags (1)
0 Kudos
Reply
3 Replies

4,007 Views
Popov_Vasil
Contributor II

Hi, Community

I'm trying to connect WiFi on the board iMX8M Plus EVK. OS is Linux 5.10.35_2.0.0 full. The output of ifconfig is givens as a file. However, trying to ping google.com, gives me a mistake: "ping: google.com: Temporary failure in name resolution". Could you show me the approach how to establish a stable WiFi connection...

Thank you!

 

 

0 Kudos
Reply

4,199 Views
joanxie
NXP TechSupport
NXP TechSupport

I have mailed to you and send you my test result, try to get it

0 Kudos
Reply

3,701 Views
kenizgandhi
Contributor III

Hello @joanxie

Even I am facing the same problem. I have connected the working ethernet cable to the board but its detecting now. But when I try to install or ping data gets lost. Can you please help me solve this issue. 

root@imx8mpevk:~# pip install python3
WARNING: Retrying (Retry(total=4, connect=None, read=None, redirect=None, status=None)) after connection broken by 'NewConnectionError('<pip._vendor.urllib3.connection.HTTPSConnection object at 0xffffb6e63670>: Failed to establish a new connection: [Errno -3] Temporary failure in name resolution')': /simple/python3/

Thank You.

Kind Regards, 

Keniz Gandhi

0 Kudos
Reply