Config Tools for i.MX custom Vid:Pid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Config Tools for i.MX custom Vid:Pid

463 次查看
eaemlogic
Contributor I

Hi!
When trying to run the DDR stress test on a device which has been fused with a custom Vid:Pid the tests fail. Performing the test on a device which has the default Vid:Pid fuses, the test succeeds. I believe that the issue is related to the sdps_comm load binary image mechanism.

0 项奖励
回复
2 回复数

458 次查看
addiyi
NXP Employee
NXP Employee

Hi,

If you are using Config tools for i.MX 25.03, you can edit the following file to use custom pid/vid

"C:\nxp\i.MX_CFG_25.06_EAR2\bin\python3\spsdk\data\devices\mimx9596\database.yaml"

 

Adrian

0 项奖励
回复

433 次查看
eaemlogic
Contributor I

That did unfortunately not do it, I see that there are some libuuu dependencies to this python back-end, maybe that has to be updated also?

0 项奖励
回复