Hi!
When trying to run the DDR stress test on a device which has been fused with a custom Vid:Pid the tests fail. Performing the test on a device which has the default Vid:Pid fuses, the test succeeds. I believe that the issue is related to the sdps_comm load binary image mechanism.
Hi,
If you are using Config tools for i.MX 25.03, you can edit the following file to use custom pid/vid
"C:\nxp\i.MX_CFG_25.06_EAR2\bin\python3\spsdk\data\devices\mimx9596\database.yaml"
Adrian
That did unfortunately not do it, I see that there are some libuuu dependencies to this python back-end, maybe that has to be updated also?