Cannot boot debian on SD card for IMX8MP evaluation board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot boot debian on SD card for IMX8MP evaluation board

494 次查看
raul22520
Contributor I

Hi, 

I am trying to boot an sd card for installing debian on my IMX8MP evaluation board (2024 version). I followed all the steps mentioned on the following instructions:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Debian-12-Installation-Guide-for-iMX8MM-...

When trying to power up the board, in SD mode, it throws the next errors:

 

 

U-Boot 2024.04-lf_v2024.04+ge3219a5a734+p0 (Feb 18 2025 - 04:03:02 +0000)

CPU:   i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)
CPU:   Commercial temperature grade (0C to 95C) at 26C
Reset cause: POR
Model: NXP i.MX8MPlus LPDDR4 EVK board
DRAM:  6 GiB
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port2 init failed, err=-19
tcpc_init: Can't find device id=0x50
setup_typec: tcpc port1 init failed, err=-19
Core:  285 devices, 36 uclasses, devicetree: separate
MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
fail to get display timings
probe video device failed, ret -19

        [0] lcd-controller@32e80000, video
        [1] mipi_dsi@32e60000, video_bridge
        [2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
fail to get display timings
probe video device failed, ret -19
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated
MMC: no card present
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Net:
Warning: ethernet@30bf0000 (eth1) using random MAC address - 86:c6:1f:7c:db:5a

Warning: ethernet@30be0000 (eth0) using random MAC address - 9a:e1:06:1e:21:9e
eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  0
Working FDT set to 43000000
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
starting USB...
Bus usb@38100000: Failed to initialize board for imx8m USB
probe failed, error -22
Bus usb@38200000: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.10
scanning bus usb@38200000 for devices... 1 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
MMC: no card present
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
MMC: no card present
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
MMC: no card present
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Can't set block device
Booting from net ...
EQOS_DMA_MODE_SWR stuckFAILED: -110BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4

 

Why is this happening? Why If I try to boot the sd card directly with fsl....wic throws the same error? If I follow all the steps, the board directly does not show anything.

0 项奖励
回复
1 回复

395 次查看
francis_guindon
Contributor I

Hello @raul22520

Have you tried with a different SD card, just to make sure it is not due to a damaged memory? Also, could you share the exact commands you used to format the SD card and copy the bootloader and kernel?

Regards,
Francis Guindon

Embedded SW Engineer at RidgeRun
Contact us: support@ridgerun.com
Developers wiki: https://developer.ridgerun.com/
Website: http://www.ridgerun.com/

Francis Guindon
Embedded SW Engineer at RidgeRun

Contact us: support@ridgerun.com
Developers wiki: https://developer.ridgerun.com/
Website: www.ridgerun.com
0 项奖励
回复