CPU is getting hang while using 3 RS485 port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CPU is getting hang while using 3 RS485 port

1,102 次查看
pankajsolanki555
Contributor I

CPU is getting hang while running the application with 3 RS485 port. Imx8 with linux 5.4.181+ is being used and CPU is getting stuck. Please help me to resolve this issue. Getting below the kernel logs : watchdog: BUG: soft lockup - CPU#0 stuck for 22s! [ 1444.538575] rcu: INFO: rcu_preempt self-detected stall on CPU [ 1444.544327] rcu: 0-....: (5248 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=2601 [ 1472.006575] watchdog: BUG: soft lockup - CPU#0 stuck for 22s! [ 1507.550574] rcu: INFO: rcu_preempt self-detected stall on CPU [ 1507.556325] rcu: 0-....: (20998 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=10386 [ 1532.006574] watchdog: BUG: soft lockup - CPU#0 stuck for 22s! [ 1570.562574] rcu: INFO: rcu_preempt self-detected stall on CPU [ 1570.568324] rcu: 0-....: (36748 ticks this GP) idle=8d6/1/0x4000000000000004 softirq=478534/478534 fqs=18170 [ 1571.810625] INFO: task jbd2/dm-0-8:375 blocked for more than 120 seconds. [ 1571.817422] Tainted: G O L 5.4.181+ #1 [ 1571.822827] "echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.

0 项奖励
回复
0 回复数