Android 14 prebuilt image problems with i.MX 8ULP EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 14 prebuilt image problems with i.MX 8ULP EVK

748 次查看
ericnelsonaz
Contributor III

Hi all,

I'm having trouble getting an Android 14 image onto a brand-new i.MX 8ULP EVK.

I've tried both the 14.0.0_1.2.0 and 14.0.0_2.0.0 images and both of them boot once and immediately reboot into recovery mode.

I'm flashing using the uuu script:

~/Downloads/android-14.0.0_2.0.0_image_8ulpevk$ ./uuu_imx_android_flash.sh -f imx8ulp -u 9x9

A log file from the serial console is attached.

Did I miss a step in the flashing or setup process?

0 项奖励
回复
1 回复

678 次查看
ericnelsonaz
Contributor III

Answering my own question.

The prebuilt image does have a problem and you'll need to build Android from sources to test it on the EVK.

0 项奖励
回复