Android 14 prebuilt image problems with i.MX 8ULP EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 14 prebuilt image problems with i.MX 8ULP EVK

722件の閲覧回数
ericnelsonaz
Contributor III

Hi all,

I'm having trouble getting an Android 14 image onto a brand-new i.MX 8ULP EVK.

I've tried both the 14.0.0_1.2.0 and 14.0.0_2.0.0 images and both of them boot once and immediately reboot into recovery mode.

I'm flashing using the uuu script:

~/Downloads/android-14.0.0_2.0.0_image_8ulpevk$ ./uuu_imx_android_flash.sh -f imx8ulp -u 9x9

A log file from the serial console is attached.

Did I miss a step in the flashing or setup process?

0 件の賞賛
返信
1 返信

652件の閲覧回数
ericnelsonaz
Contributor III

Answering my own question.

The prebuilt image does have a problem and you'll need to build Android from sources to test it on the EVK.

0 件の賞賛
返信