imx6q mfgtools for android_N7.1.2_2.0.0 not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q mfgtools for android_N7.1.2_2.0.0 not work

imx6q mfgtools for android_N7.1.2_2.0.0 not work

Hi nxp,

     imx6q  mfgtools not work, can't open;

     I download the mfgtools for android 7.1.2_2.0.0, but the size of mfgtools.zip only 4.28Mbytes, the sub dir is clean, no firmware and ucl;

    the download from this: https://www.nxp.com/webapp/sps/download/preDownload.jsp 

thanks

Comments

Hello,

 

  As has been mentioned in Community discussion “imx6q mfgtools for

android 7.1.2_2.0.0 problem”, linked below, N7.1.2. MFG tool package

on the Web does not contain images for target loading. Customers can

use "Android_Quick_Start_Guide.pdf", section 3.3 (Flashing board images) how

to use files from OS (demo) images.

https://community.nxp.com/message/957626 

 

  Also, files ucl2.xml and mksdcard-android.sh.tar should be located

in mfgtools\Profiles\Linux\OS Firmware\ directory.

The files may be taken from the previous mfgtool release.

 

Regards,

Yuri.

Hello   Yuri Muhin,

           partition-table.img is the new img file on andorid 7.1.2 release;  but the ucl2.xml from the previous mfgtool release not have, so the partition-table.img not flashing to the board;

        

     the borad can not bring up after flashing with the previous mfgtool, can't find partition:boot

   this is the log:


U-Boot 2017.03 (Sep 20 2017 - 00:38:39 +0800)

CPU: Freescale i.MX6Q rev1.5 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 38C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:2
Net: No ethernet found.
can't find partition: misc, dump the partition table
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='bootloader' start=2 len=2046
idx 2, ptn 1 name='mmcsdc1' start=16384 len=65536
idx 3, ptn 2 name='mmcsdc2' start=83968 len=65536
idx 4, ptn 0 name='' start=0 len=0
cannot get the partion info for misc
Cannot find partition 4080
do_raw_read failed, ret 1
read_bootctl, bcb_rw_block read failed
read command failed

Hello,

  I will inform the team about the issue.

Thanks for Your information!

Regards,

Yuri.

No ratings
Version history
Last update:
‎11-01-2017 09:56 PM
Updated by: